cancel
Showing results for 
Search instead for 
Did you mean: 

T2T Emulation Response Failure

LltWc
Senior

I'm working on emulating a T2T with my device. It successfully makes it through automatic anticollision, then starts looking for commands. When I see 0x30 0x00, I go ahead and send the first 16 bytes, but the reader does not react or show the read data.

LltWc_0-1727819257864.png

Right now I'm thinking that I'm transmitting wrong while in Listen Mode. The RFAL never does T2T emulation, so I don't have an example there. Right now, when I see a 0x30 command, I do the following:

Send command CLEAR FIFO

Set Num Tx Bytes 1 to the MSB

Set Num Tx Bytes 2 mask 0xF8 to the LSB

Write the data to the FIFO

Send command TX WITH CRC

Is there a different way to do it in Listen Mode? With T2T Emulation the chip's field will never be on, but I don't see a way to explicitly modulate a response. The first 16 bytes are shown above, with the CC 0xE1 0x10 0x3F 0x0F. I do also have an empty NDEF TLV and the Terminator TLV, but no memory regions beyond the first 4 blocks are attempted to be read.

Also - I couldn't find any information on the INT2 byte after the second BCC, so I copied the 0x48 I've seen on NTAGs. What does that byte represent?

 

This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14

Hi LltWc,

honestly, don't know with this macroscopic view. You need to debug by:

  1. Some NFC reader device (e.g. the mentioned) debug tabs which allow you to 
    • Verify all the state changes and FWT timings inside your tag implementation
    • Assess the operating volume - look for holes, etc.
  2. Trace the communication with the phone (NFC sniff and/or Logic analyzer of ST25R comm).
    • Identify sequences which are not implemented in you software
    • See timing which may not have been fulfilled.

For commands not understood I would typically mute (i.e. not send a response). For commands per T2T protocols I would then return a 4bit NACK (e.g. the mentioned 0000).

Could be that you are not handling the Removal Procedure of the phone correctly. I would assume a HLTA->WUPA sequence. With the HLTA your software needs to issue the GOTO_SLEEP direct command. But also many other things which might happen. With the little information you are essentially blind.

Ulysses

Understood, thanks. I improved some of the state transitions and resolved a hardware issue that was affecting the antenna range and now I can read pretty consistently with a Pixel 6a, but not with a Galaxy Fold or iPhone.

Also, a few questions on the ST25R3916 Discovery GUI, as the user manual doesn't go into detail:

  • In the "Polling" tab, my device does not show up as a found tag. However, if I uncheck "Ignore tag fragments", it does show up. What is a tag fragment, and how does it differ from a full tag?
  • In the "ISO 14443A" tab, when I send a REQA, it responds "no anticollision, ATQA: 0044, REQA[NotSupported]". Is this saying that anticollision does not occur despite getting the ATQA?
  • In the "NFC Type 2" tab, I also get a "NotSupported" error. What does that mean specifically?

Hi,

Inside the ATQA there are fields where a tag should indicate if bitwise anticollision is supported. I think you swapped the bytes in your ATQA, should be 4400, the 44h should be transmitted first.

So it is showing it as a tag fragment as no UID could be received.

BR, Ulysses

 

 

Well, this is embarrassing, but that was it. I messed around with ATQA order when I was initially populating PT_MEM because I wasn't sure which went first, but I had left it alone since then.

Now it works with all three test phones: Pixel 6a, Galaxy Fold4, iPhone 14. (Flipper Zero seems to break something, but that's likely because it doesn't respect the tag information as part of anticollision since it's just a hobbyist device.)

Question on the documentation, then. The NFC Forum Digital Protocol specifies Byte 1 of the SENS_RES/ATQA as the one with size (0x44), and Byte 2 as T1T stuff (0x00). The ST25R3916 datasheet specifies that the SENS_RES is bytes 10 and 11, but in the order [2:1]. I interpreted this as meaning 0x00 goes first, then 0x44. Is that the incorrect interpretation, or is the datasheet wrong?

LltWc_0-1728416166320.png

 

Hi,

 

I think no order swap was intended in the text here and it just goes naturally out: Byte 10 being the first ATQA byte and byte 11 being the second ATQA byte. 

I admit that this detail is not well written on the doc.

BR, Ulysses