2020-09-02 4:21 AM
Hello,
using STSW-ST25RFAL002 to version 0x020200U (RFAL Current Version: v2.2.0) I encountered a problem in card emulation mode, practically the state machine remaine blocked on the RFAL_NFC_STATE_LISTEN_ACTIVATION state indefinitely rfal_nfc.c: 518 the rfalNfcListentivation() function always return ERR_BUSY.
This happened to me with several Android smartphones (with iPhone 2020 se no problem).
I solved it by adding this patch:
--- a/STSW-ST25RFAL002/source/rfal_nfc.c
+++ b/STSW-ST25RFAL002/source/rfal_nfc.c
@@ -516,6 +516,13 @@ void rfalNfcWorker( void )
/*******************************************************************************/
case RFAL_NFC_STATE_LISTEN_ACTIVATION:
+ if( platformTimerIsExpired( gNfcDev.discTmr ) ) /* Check if the total duration has been reached */
+ {
+ rfalListenStop();
+ gNfcDev.state = RFAL_NFC_STATE_START_DISCOVERY; /* Restart the discovery loop */
+ rfalNfcNfcNotify( gNfcDev.state ); /* Notify caller */
+ break;
+ }
case RFAL_NFC_STATE_LISTEN_SLEEP:
err = rfalNfcListenActivation();
If you have a better way of solving the problem I will be happy to apply it, I am not happy to have to bring patch to the third party library.
Thanks so much,
D.
Solved! Go to Solution.
2021-04-19 10:30 AM
Hi pagano.paganino,
could you share a logic analyzer trace of the issue?
On which platform is your source running? NUCLEO-L476 + X-NUCLEO-NFC06A1?
Regards, Ulysses
2021-04-19 10:46 AM
Hi Ulysses,
could you share a logic analyzer trace of the issue?
I ordered it, as soon as it arrives with pleasure
On which platform is your source running? NUCLEO-L476 + X-NUCLEO-NFC06A1?
NUCLEO-WB55 + X-NUCLEO-NFC06A1
Thanks and regards,
D.
2021-04-20 5:27 AM
Hi pagano.paganino,
I think I have all the hardware available - including iPhone SE 2020. If you provide a binary/hex (which includes the logging), I could give it a try.
Regards, Ulysses
2021-04-20 2:34 PM
Hi Ulysses,
attached the firmware for the nucleo-wb55 + x-nucleo-nfc06a1.
after finishing the flashing procedure:
if everything goes well you can see:
MicroPython v1.15-2-g6e0f9b926-dirty on 2021-04-20; NUCLEO-WB55 with STM32WB55RGV6
Type "help()" for more information.
>>>
NUCLEO-WB55
SPI(1, baudrate=8000000, polarity=0, phase=1, bits=8)
Pin(Pin.cpu.A4, mode=Pin.OUT, pull=Pin.PULL_UP)
Pin(Pin.cpu.C0, mode=Pin.IN)
At this point everything is ready, in the software I have included an emulation of uri ndef pointing to the site https://community.st.com
and enabled logging for:
rfalBitRate bitRate;
bool isDataRcvd;
rfalLmState lmSt = rfalListenGetState( &isDataRcvd, &bitRate );
err = rfalNfcListenActivation();
printf("la: %d lgs: %d isdr: %d br: %d\n", err, lmSt, isDataRcvd, bitRate);
Thanks for all, regards.
D.
2021-04-21 11:19 PM
Hi pagano.paganino,
in my exeriments the iPhone SE 2020 always opened the URI. However using Samsung Galaxy S21 I see an immediate hang.
SPI trace shows the interrupt is stopped to be handled at some point, afterwards IRQ is constant high and no more SPI traffic:
Zoomed in a bit more to see the last frames:
I would suspect damaged locking of SPI (platform(Un)Protect...(). I would assume that it depends on timing - if interrupt comes while an SPI transfer is ongoing. That's maybe why it is happening with the iPhone at your side but not at mine.
Regards, Ulysses