2022-10-24 11:31 AM
According to the ST25DVi2c datasheet, a high bitrate encoding has four subcarrier pulses (followed or preceded by 9.44us of unmodulated time) to designate a 0 or 1. A low bitrate uses 16 pulses and 37.76us of unmodulated time.
By changing bits 3 and 4 of the Stream mode definition register, I've been able to configure the st25r3916 for either bit rate. The datasheet, however, offers "# of pulse" values of 1, 2, 4, or 8. I believe that it should read 1, 2, 4, or 16. Am I correct?
Best,
Oliver
Solved! Go to Solution.
2022-11-02 02:21 AM
Hi Oliver,
you are mistaking the Appendix A: It merely describes how the coding of the responses to the fast commands is performed, it does not describe the normal responses:
To my knowledge all command codes which start with 0xC. are fast commands which are answered with a doubled response data rate.
How do you evaluate "able to communicate"? Which commands did you execute with which request flags. Just because you get some bytes into the FIFO does not necessarily mean that you are getting a full frame which also can be decoded correctly.
BR, Ulysses
2022-10-24 11:50 PM
Hi Oliver,
IMO the 8 is correct. Beware of the naming of the data rates. What you are referring is both "high":
BR, Ulysses
2022-10-25 01:21 PM
Thank you for your reply, Ulysses. Page 159 of the st25dvi2c datasheet outlines the two "data rates", one is "low" and the other is "high". This is the terminology the datasheet uses. They are used for regular and fast commands respectively. I understand that they both use the same frequency of subcarrier, and that their distinction is in the number of pulses within a pulse period. Low uses 16, and high uses 4.
I have been able to communicate with both fast and regular commands by changing the # of pulses register in the ST25R3916 between "4" and "8". So I feel there is some discrepancy between the ST25r3916 and st25dvi2c datasheets, given that I have been able to communicate using either command type.
2022-11-02 02:21 AM
Hi Oliver,
you are mistaking the Appendix A: It merely describes how the coding of the responses to the fast commands is performed, it does not describe the normal responses:
To my knowledge all command codes which start with 0xC. are fast commands which are answered with a doubled response data rate.
How do you evaluate "able to communicate"? Which commands did you execute with which request flags. Just because you get some bytes into the FIFO does not necessarily mean that you are getting a full frame which also can be decoded correctly.
BR, Ulysses