cancel
Showing results for 
Search instead for 
Did you mean: 

ST25RU3993HPEV - suddenly not detecting tag

spp.1
Associate

I have been using the ST25RU3993HPEV board for the Tag detection. Earlier the board is performing well and it was detecting tag. But suddenly reader is not detecting tag.

Is there any chance for power amplifier regulator has gone bad?

If the tag is kept on the surface of the antenna, it will be detected at some point.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bart Herse
Senior II

Dear SPP.1

is the supply voltage for the power amplifier still present? --> check voltage between pin 1 and 2 on J21. Note to switch on the RF before doing the this measurement.

Is the HPEV reader still able to detect tags, when switching to the internal power amplifier?

Cheers,

B

View solution in original post

1 REPLY 1
Bart Herse
Senior II

Dear SPP.1

is the supply voltage for the power amplifier still present? --> check voltage between pin 1 and 2 on J21. Note to switch on the RF before doing the this measurement.

Is the HPEV reader still able to detect tags, when switching to the internal power amplifier?

Cheers,

B