cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3914-AQWT MISO signal is shifted to 1.2V

PSHAH.1
Associate

I am Using ST25R3914-AQWT NFC chip as a Slave Device and Renesas RL78 as Master device for SPI communication. 

When I tried to interface both controller MISO signal is shifted to 1.2V

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Travis Palmer
ST Employee

Hello PSHAH.1,

A schematic diagram would be indeed helpful.

Our chip sets typically have the VDD_IO supply. It sources the internal level shifter. VDD_IO should be at the MCUs SPI level.

e.g. if the MCU is running at 3.3V, also VDD_IO should be put to 3.3V. VDD of the ST25R can be set to any value specified in the datasheet.

If the MCU is supplied via 3.3V and VDD_IO is driven by 5V, it could explain a shift in the MISO signal.

please let me know, if this helped!

BR Travis

View solution in original post

3 REPLIES 3

Would suggest you're wiring it wrong.Show a wiring diagram or schematic. ​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Travis Palmer
ST Employee

Hello PSHAH.1,

A schematic diagram would be indeed helpful.

Our chip sets typically have the VDD_IO supply. It sources the internal level shifter. VDD_IO should be at the MCUs SPI level.

e.g. if the MCU is running at 3.3V, also VDD_IO should be put to 3.3V. VDD of the ST25R can be set to any value specified in the datasheet.

If the MCU is supplied via 3.3V and VDD_IO is driven by 5V, it could explain a shift in the MISO signal.

please let me know, if this helped!

BR Travis

PSHAH.1
Associate

Thank you for reply this issue is resolved. there was some stack issue now SPI is working perfectly ok