2023-11-27 01:19 AM - edited 2023-11-27 01:38 AM
Hello,
I successfully succeed to control my ST25RU3993-HPEV with my external MCU.
I can detects all my tags just in a area of 10 cm, but my External PA is activated. I don't know what parameters i have to change to allows at my system to detect my tags in a area of 10 m ?
I also see a consumption of 0.7 A so i think that the PA is running good.
And i use the default parameter in the FW wich is on this link
Someone can help me pls ?
Thanks you !
Paul 🙂
2024-01-08 01:36 AM
Hello Paul,
which tags and which reader antenna are you using?
Best regards,
Marcel