2022-09-13 9:44 AM
At ST25RU3993-HPEV firmware how to control an antenna distance? For eg. I want an antenna to read tags in 3ft only.
Solved! Go to Solution.
2022-10-14 6:15 AM
Hello YChav.3
In general the read range can be limited with the TX power settings. The less Tx power the less read range. A strong dependency is also given through the used antenna. Also the used Tag and frequency can have a impact on the read range. This means one Tx power settings can limit the read range for one setup, but could allow to read further with a different setup.
BR
Nick
2022-10-14 6:15 AM
Hello YChav.3
In general the read range can be limited with the TX power settings. The less Tx power the less read range. A strong dependency is also given through the used antenna. Also the used Tag and frequency can have a impact on the read range. This means one Tx power settings can limit the read range for one setup, but could allow to read further with a different setup.
BR
Nick