cancel
Showing results for 
Search instead for 
Did you mean: 

ST25RU3993 eval low output level

MPrzy.1
Associate

Hello,

I've observed that output level on both antenna port is lower than is specified in datasheet. I've checked it on two eval boards. Below results:

For internal PA: (output level set/ measured level/ detector voltage

  1. -12 / 4,5 dBm / 0 ,71V
  2. -6 / 8,9 dBm / 0,81V
  3. 0 / 12,2 dBm /0,89V

For external PA:

  1. -12 / 14,4 dBm , / 0,92V
  2. -6 / 19,5 dBm / 1,05V
  3. - 3 / 20,8 dBm / 1,08V
  4. 0 / 21,5 dBm / 1,1V

In both cases output level is lower by 7-8 dBm that expected. Any suggestion?

Best Regards, Michał

1 ACCEPTED SOLUTION

Accepted Solutions
MPrzy.1
Associate

Problem probably solved and was in my spectrum analyzer malfunction.

Michal

View solution in original post

1 REPLY 1
MPrzy.1
Associate

Problem probably solved and was in my spectrum analyzer malfunction.

Michal