2020-03-03 4:26 AM
I'm running a ST25RU3993-EVAL with firmware version V2.0.0.0 STUHFL. Under "Reader Settings" in tab "Settings" under "EU Profile", within the TX-Options, there is a Selection-Field "Internal/External PA", which by default is set to external PA.
When I try to set this to internal PA, I do get an error message "TX setting failed".
Has anyone an idea, if this feature is possibly disabled by firmware, or even not yet implemented?
Solved! Go to Solution.
2020-03-05 12:51 AM
Hi,
thank you for this hint!
We could reproduce this issue and in the next GUI Version 2.0.2.0 it will be possible to switch between the Internal/External PA.
Best regards,
Marcel
2020-03-05 12:51 AM
Hi,
thank you for this hint!
We could reproduce this issue and in the next GUI Version 2.0.2.0 it will be possible to switch between the Internal/External PA.
Best regards,
Marcel
2020-03-05 1:53 AM
Hi,
and thanks a lot for the response!
I'm looking forward to testing the next GUI release ...
Best regards,
KFIN