cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R95 detect ST25D tag

Eyzeryong
Associate III

I use ST25R95 to detect the ST25D tag. I keep the tag on the antenna of the Reader all the time, and some situations have occurred.

Hi

Even if I place it precisely on it all the time, the tag may not be read probabilistically during detection. Is this normal? The antenna fails to read the tag about two or three times out of ten readings.

Please help me,thanks~

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hi,

Based on your inductance value of 0.46uH, I populated the respective values from your design into the Excel calculation tool, and this is what I obtained:

 

Blake_Victor_1-1737116548330.png

Following the steps from the application note, I replaced the inductance value, and the chart looks like this:

Blake_Victor_2-1737116578300.pngBlake_Victor_3-1737116584937.png

 

From your matching network, try to modify the following:

  • C18 + C19 = 270pF
  • C16, C21 = 56pF
  • BC1, BC2 = 280nH
  • C20, C17 = 200pF

The tuning frequency can be adjusted using C2, and the impedance magnitude can be adjusted using C11/C12.

BR,

BV

 

View solution in original post

12 REPLIES 12
Brian TIDAL
ST Employee

Hi,

do you use your own custom board or one of the ST demo boards (if yes, which one)? 

What is the sequence of command being sent and what is the return code in case of failure? I would suggest to connect a logic analyzer on SPI + IRQ_IN and IRQ_OUT and provide the trace file.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi, 

    thanks for your answer~

   I use own custom board, and ues ISO15693,send these define:

ISO15693_REQFLAG_SINGLESUBCARRIER,
ISO15693_REQFLAG_HIGHDATARATE,
ISO15693_REQFLAG_INVENTORYFLAGSET,
ISO15693_REQFLAG_NOPROTOCOLEXTENSION,
ISO15693_REQFLAG_NOTAFI,
ISO15693_REQFLAG_1SLOT,
ISO15693_REQFLAG_OPTIONFLAGNOTSET,
ISO15693_REQFLAG_RFUNOTSET

by 0x04 SendRecv cmd

sometimes host return me 0x87 Frame wait time out or no tag,but I still put the tag on the antenna,I've been aiming at it all the time,I don't know why....,

I am sorry that I haven't the logic analyzer,so I couldn't offer you more about SPI + IRQ_IN and IRQ_OUT

I use 0x09046801011D to initialize ISO15693

 

Brian TIDAL
ST Employee

Hi,

This is probably due to a matching circuit issue on the custom board. Make sure to follow the "Step by step procedure" described in the Application Note AN5248 (ST25R95 transceiver antenna tuning circuit with EMI filter) to properly tune the matching circuit.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello

I have download the ST25R95 EMI FILTER CALCULATION.xlsm,but I observed that I'm a little bit unproductive

Eyzeryong_0-1736904821332.png

This is my part of the schematic, could you help me take a look, thank you so much

 

Hi

I'll add a little something,My board has an antenna coil turn of 2, which is a 46mm square。

 

Hi,

Based on the antenna parameter you defined (0.48uH), different Low Pass Filter values and some tuning in the matching circuit are required.

According to your inductance value, try adapting similar Low Pass Filter values as described in the Application Note: AN5248.  Additionally, tune the capacitance values of C11, C12, and C2 to achieve a similar impedance chart as shown below:

Blake_Victor_0-1737040766448.png

I hope this helps with your matching circuit.

Regards,

BV

Thank you for helping me with this chart

is any advise on my broad?I have not any clue to solve my question

thanks

Hi

I actually measured the inductance of the coil to be 0.46uH instead of 0.48uH, what changes do I need to make to my capacitance?

Hi,

Based on your inductance value of 0.46uH, I populated the respective values from your design into the Excel calculation tool, and this is what I obtained:

 

Blake_Victor_1-1737116548330.png

Following the steps from the application note, I replaced the inductance value, and the chart looks like this:

Blake_Victor_2-1737116578300.pngBlake_Victor_3-1737116584937.png

 

From your matching network, try to modify the following:

  • C18 + C19 = 270pF
  • C16, C21 = 56pF
  • BC1, BC2 = 280nH
  • C20, C17 = 200pF

The tuning frequency can be adjusted using C2, and the impedance magnitude can be adjusted using C11/C12.

BR,

BV