Hi,Thank you for the information you have provided.After reviewing it, I noticed that the capacitor package size highlighted in yellow is different from the others. Could you please explain the reason for using a different package size for these capa...
Hi,Yes, you have filled with correct value. Please check with the Smith chart to ensure the values are correct. If you need to fine-tune the values, you can adjust them accordingly. BR,BV
Hi,After importing the antenna parameters (values you provided), the impedance chart you get doesn't match the simulation output, which still needs fine-tuning.Reason: You might have misplaced the components or used different values. Please re-check ...
Hi,Based on your inductance value of 0.46uH, I populated the respective values from your design into the Excel calculation tool, and this is what I obtained: Following the steps from the application note, I replaced the inductance value, and the char...
Hi,Based on the antenna parameter you defined (0.48uH), different Low Pass Filter values and some tuning in the matching circuit are required.According to your inductance value, try adapting similar Low Pass Filter values as described in the Applica...