cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3916 FIFO read strange issue (Nucleo-L433RC-P & X-Nucleo-NFC06A1)

OSilv.1
Associate II

After I write to the FIFO, I read the FIFO to check if the bytes were property transferred (I understand that I cannot read and then transmit, this is just for debugging). I have a strange issue where the number of bytes in the FIFO are exactly half of what I write. Also, the bytes themselves are not what I wrote. Each time I read from the FIFO, the number of bytes in the FIFO are halved until there are zero bytes.

Here I write to the FIFO:

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_RESET);

ret = HAL_SPI_Transmit(&hspi2, &FIFO_w, 1, 50);

ret = HAL_SPI_Transmit(&hspi2, &sof, 1, 50);

ret = HAL_SPI_Transmit(&hspi2, ppm_message, ppm_message_len, 50);

ret = HAL_SPI_Transmit(&hspi2, &eof, 1, 50);

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_SET);

And here I read the FIFO length and FIFO itself:

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_RESET);

ret = HAL_SPI_Transmit(&hspi2, &FIFO_status_addr_r, 1, 50);

ret = HAL_SPI_Receive(&hspi2, &raw_rx_len, 1, 50);

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_SET);

uint8_t raw_rx[raw_rx_len];

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_RESET);

ret = HAL_SPI_Transmit(&hspi2, &FIFO_r, 1, 50);

ret = HAL_SPI_Receive(&hspi2, raw_rx, raw_rx_len, 50);

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_SET);

ppm_message[24] is: {0x20, 0x02, 0x02, 0x02, 0x08, 0x80...}

raw_rx[12] is: {0x10, 0x90, 0x01, 0x01, 0x01, 0x04, 0x40...}

the next FIFO read produces:

raw_rx[6] is: {0x01, 0x01, 0x01, 0x01, 0x04, 0x40}

and then:

raw_rx[3] is: {0x40, 0x40, 0x40}

and so on...

Its strange that the raw_rx looks vaguely like the ppm_message in terms of the pattern of repeated numbers.

Any help or guesses would be greatly appreciated!

Thanks,

Oliver

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee

Hi Oliver,

shifted bit patterns indicate a wrong SPI mode being used. Please check that.

Best Regards, Ulysses

View solution in original post

2 REPLIES 2
Ulysses HERNIOSUS
ST Employee

Hi Oliver,

shifted bit patterns indicate a wrong SPI mode being used. Please check that.

Best Regards, Ulysses

This was it. Working now with CPOL = Low and CPHA = 2 Edge.

Thank you!