2022-12-19 7:54 PM
Hello, I am trying to open a project that can turn on the low power MCU stm32l031 with ANT7-T-25DV64KC while turning high and low periodically for GPO pin of the MCU. I tried many different ways but still not done with any of them (steval code and using NFC4 and 7 provided by stm32cubeide).
Would you please suggest me for any reference or sample for St25DV-i2c?
Solved! Go to Solution.
2023-01-30 7:59 AM
Hello,
It is good news that after updating my cubeIde to 1.11.2. It is working now. Therefore, I modified EH project code to detach the BSP button and LEDs while it is always working in EH mode (Active boot).
For EH project, I have one more question. As you told me EH_mode is nonvolatile, if I already set ST25DVxxKC_EN_STATUS_E = ST25DVXXKC_ENABLE and ST25DVxxKC_EH_MODE_STATUS_E = ST25DVXXKC_EH_ACTIVE_AFTER_BOOT for my extension board ST25 chip, can I remove MX_NFC7_EH_Process (as in my case, I will not turn off EH function).
And for NDEF example, I have some questions.
It is very interesting that by this strcpy function, can directly change the payload length and set other headers. What is the URI_ID for MME (Text, in my RF430 code, I use 0x02, // URI header identifier). And furthermore, what is the difference between URI_Message and Information. It is a bit confused as I originally used TI chip for NFC.
In my case, I want to send ADC sensor values in TEXT format when I put my mobile phone to my ST25.
I will attach my RF430 NDEF format.
const u08_t NFC_NDEF_Message[57] = {
// Block 0
0xE1, // NDEF Magic Number
0x40, // Version Number, read/write access conditions
0x79, //0x7E, // 1008 bytes / 8 = 126 blocks
0x00,//0x04,//8 byte extended memory //0x00, // does not support read multiple blocks (limited to only 3 blocks)
// Block 1
0x03, // NDEF Message present
0x34, // Length , 17 bytes
0x91, // Record header
0x01, // type length
// Block 2
0x0E, // Payload length 14
0x54, // Record Type T (Text)
0x02, // URI header identifier
0x65, // 'e'
// Block 3
0x6E, // 'n'
0x54, // 'T'
0x65, // 'e'
0x6D, // 'm'
// Block 4
0x70, // 'p'
0x74, // 't'
0x75, // 'u'
0x72, // 'r'
// Block 5
0x65, // 'e'
0x3A, // ':'
0x00,
0x00,
// Block 6
0x51, // Record header
0x01, // type length
0x0B, // Payload length 11
0x54, // Record Type T (Text)
// Block 7
0x02, // URI header identifier
0x65, // 'e'
0x6E, // 'n'
0x4E, // 'N'
// Block 8
0x48, // 'H'
0x34, // '4'
0x2B, // '+'
0x3A, // ':'
// Block 9
0x00, //
0x00, //
0x00,
0x51, // Record header
// Block 10
0x01, // type length
0x0A, // Payload length
0x54, // Record Type T (Text)
0x02, // URI header identifier
// Block 11
0x65, // 'e'
0x6E, // 'n'
0x43, // 'C'
0x6C, // 'l'
// Block 12
0x2D, // '-'
0x3A, // ':'
0x00, //
0x00, //
// Block 13
0x00, //
0xFE, // TLV terminator
0x00, // Empty don't care
0x00 // Empty don't care
};
Thank you for reading.
2023-01-30 8:42 AM
The problem is solved but, I still want your answers for the questions.
For EH project, I have one more question. As you told me EH_mode is nonvolatile, if I already set ST25DVxxKC_EN_STATUS_E = ST25DVXXKC_ENABLE and ST25DVxxKC_EH_MODE_STATUS_E = ST25DVXXKC_EH_ACTIVE_AFTER_BOOT for my extension board ST25 chip, can I remove MX_NFC7_EH_Process (as in my case, I will not turn off EH function).
And for NDEF example, I have some questions.
And furthermore, what is the difference between URI_Message and Information. It is a bit confused as I originally used TI chip for NFC.
2023-01-30 9:30 AM
Hi @WPARK.1,
Great that you solved your issue, Happy for you.
I hope this can help you.
Kind Regards.