2021-08-03 3:26 AM
Hello all
I use ST25DV64K.
If the I2C communication is normal, it returns ACK after receiving data, and after receiving the last data, it returns NACK response and issues Stop Condition.
If the I2C communication is abnormal, and the master issues a stop condition without returning a NACK response to the NFC tag, will the NFC tag be able to receive the stop condition normally?
Also, after the Stop Condition is issued, will the NFC tag be able to accept the next Start Condition normally?
Or will it not accept the next input data until the maximum value of TCHCL or TCLCH (25ms) has elapsed?
BR
Morooka
Solved! Go to Solution.
2021-08-04 6:50 AM
Dear Morooka,
In a normal I2C read transaction, the master is signaling to the slave that it doesn't want to read more data by sending a NACK on the 9th bit of the last byte received from the slave.
On the contrary, the master is signaling to the slave that it wants to read one more byte by sending a ACK.
If the slave is receiving a ACK, it means that it has to deliver one more byte. So, after the ACK condition, it will start to present the next byte on the next clock rising edge.
So, if the master is not sending a NACK, but instead is sending a ACK and then a STOP, here is what can happen: on the rising edge of the clock following the ACK, the slave will present on the bus the first bit of the next byte in memory (MSB bit)
Then, there is two possible cases:
So, it is definitely a bad idea to send a ACK after last byte read and before the STOP, but in any case the situation will be recovered after 25ms thanks to the internal timeout of the ST25DV.
Hope this help and best regards.
2021-08-04 6:50 AM
Dear Morooka,
In a normal I2C read transaction, the master is signaling to the slave that it doesn't want to read more data by sending a NACK on the 9th bit of the last byte received from the slave.
On the contrary, the master is signaling to the slave that it wants to read one more byte by sending a ACK.
If the slave is receiving a ACK, it means that it has to deliver one more byte. So, after the ACK condition, it will start to present the next byte on the next clock rising edge.
So, if the master is not sending a NACK, but instead is sending a ACK and then a STOP, here is what can happen: on the rising edge of the clock following the ACK, the slave will present on the bus the first bit of the next byte in memory (MSB bit)
Then, there is two possible cases:
So, it is definitely a bad idea to send a ACK after last byte read and before the STOP, but in any case the situation will be recovered after 25ms thanks to the internal timeout of the ST25DV.
Hope this help and best regards.
2021-08-18 10:54 PM
Thanks @JL. Lebon_O (ST Employee)
I understood that ST25DV Communication error when reading I2C
Thank you.
Best regards.