2021-03-01 11:32 PM
STM32L476VG is the MCU we are interfacing with ST25R3911B using SPI.
what we have understood from some search is that we need RFAL (abstraction layer) to interface with RF HAL.
Then once we integrate RFAL and RF HAL in our system workbench(ac6) project we need to build the integration then use SPI calls to read the register from RFID reader ST25R3911B
we wanted to use ISO-14443A standard to be configured and read the values.
where do we get the basic RFAL work space or code flow so that we shall use in our current project?
Kindly guide us and let us know are we in right path?
Solved! Go to Solution.
2021-05-21 02:56 AM
2021-05-21 02:57 AM
2021-05-21 02:58 AM
Hi BT,
let me know if these connections are fine.
regards
Ravi
2021-05-21 03:27 AM
Hi,
disconnect the ST25R3911B IRQ pin from the STM32L476VG-DISCO board and probe the IRQ on the X-NUCLEO-NFC05A1 with a scope (CN8 pin 1) : when resetting the MCU, you should see a falling interrupt just after few SPI exchanges following the MCU reset.
Do you see the interrupt?
Rgds
BT
2021-05-21 03:41 AM
Hi BT,
No we are not seeing any activity after removing PA3 and connecting to CN8 pin 1 on the NFC side.
regards
Ravi
2021-05-21 04:35 AM
Hi BT,
SPI init is succeeding whereas INT i s failing what could be the issue??..hardware NFC05A1...then how do we proceed from here??,,kindly help us on this.
regards
Ravi
2021-05-21 04:50 AM
Hi,
is the Gnd properly connected on the scope probe?
Can you confirm that you have press the B1 reset push button on the STM32L476VG-DISCO while probing?
is the CN8.1 pin high or low?
Have you properly connected ST25R3911B VDD_IO and VDD power supply?
Rgds
BT
2021-05-21 05:09 AM
Hi BT,
1.Yes, the GND is connected properly on the scope probe.
2.Yes we have pressed the B1 reset push button on the STM32L476VG-DISCO.
3.CN8.1 pin is low
4.Yes we are seeing the green light in ST25R3911B board..we are seeing SPI init passed as mentioned earlier.
regards
Ravi
2021-05-21 05:18 AM
2021-05-21 05:18 AM
Hi BT,
we are also getting MOSI and MISO line ...