2014-03-05 12:04 PM
Hi.
I am using CR95HF. I need to identify the presence of multiple iso15693 tags ( placed on the same time ). I need to know how the amount of tags only. Is ther a command or algorithm ?. Please Advise. Ephraim Oved #cr95hf-iso15693 #m24lr #cr95hf #multi-tag #collisionSolved! Go to Solution.
2014-03-06 04:08 AM
Hello,
Are you using our software in order to control CR95HF?The inventory algorithm 16 slots is implemented inside.If not, inventory command is serving this aim; it is needed to control it. In order to detect presence of many tags , it is needed to send an inventory 1 slot with a zero masklength value.Have a nice day,
Best regards,ST NFC/RFID Dynamic tag online support2014-03-06 04:08 AM
Hello,
Are you using our software in order to control CR95HF?The inventory algorithm 16 slots is implemented inside.If not, inventory command is serving this aim; it is needed to control it. In order to detect presence of many tags , it is needed to send an inventory 1 slot with a zero masklength value.Have a nice day,
Best regards,ST NFC/RFID Dynamic tag online support