cancel
Showing results for 
Search instead for 
Did you mean: 

Powering the STM32L476RG board from the EH pin of the ST25DV

FGang
Associate II

How can I power the STM32L476RG board via the EH pin of the ST25DV? Is there a module for this?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Yes, you can supply an STM32L476RG via the EH pin of an ST25DV if:

  • you have observed the note on pin V_EH in the data sheet: This analogue output pin is used to deliver the analogue voltage V_EH available when the Energy harvesting mode is enabled and if the RF field strength is sufficient. [...] Energy harvesting voltage output is not regulated.
  • The last sentence indicates that you connect a voltage regulator downstream, like e.g. in the STEVAL-SMARTAG2, which can generate the VCC for the STM32L476. It makes sense for this voltage to be as low as possible (in STEVAL-SMARTAG2 = 1.9V) so that even weaker NFC fields are able to supply the STM32. Of course, you must design the entire board for ultra-low power so that other consumers do not cause the voltage to collapse. The STM32L476 program must also be carefully optimised for minimum power consumption.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Yes, you can supply an STM32L476RG via the EH pin of an ST25DV if:

  • you have observed the note on pin V_EH in the data sheet: This analogue output pin is used to deliver the analogue voltage V_EH available when the Energy harvesting mode is enabled and if the RF field strength is sufficient. [...] Energy harvesting voltage output is not regulated.
  • The last sentence indicates that you connect a voltage regulator downstream, like e.g. in the STEVAL-SMARTAG2, which can generate the VCC for the STM32L476. It makes sense for this voltage to be as low as possible (in STEVAL-SMARTAG2 = 1.9V) so that even weaker NFC fields are able to supply the STM32. Of course, you must design the entire board for ultra-low power so that other consumers do not cause the voltage to collapse. The STM32L476 program must also be carefully optimised for minimum power consumption.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.