2023-09-16 1:31 AM
I should make an application with NFC where the entire circuit is powered by energy harvesting.
For this reason I thought of using the ST25DV and I have already purchased the X-NUCLEO-NFC07A1 and X-NUCLEO-STM32L476RG.
I have successfully obtained the energy harvesting of the antenna and can light the LED, now I want to use the energy of the antenna to wake up the MCU (L476), what do I need to do?
I have tried to connect VCC with EH pin, but L4 is not waking up, what should I do to power the antenna to the MCU (L476) instead of the ST-LINK USB
Solved! Go to Solution.
2023-09-26 3:32 AM
2023-09-26 3:32 AM
Hi,
please refer to https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/energy-harvesting-on-st25dv-i2c-04k-with-stm32l476-mcu/td-p/54135
Best Regards,
BB