Hi ,The error code 5 is not a value that the ST25TV02K PresentPassword RF command is returning. So we would need to know which subfunction of the rfalST25xVPollerPresentPassword is generating this error.Also could you please provide the values of A1S...
Hi Fabrice,by 'M24SR selected from the RF side', it is meant that the M24SR has been activated - meaning the phone has performed the technology detection, collision resolution, device activation). As you have indicated the new NDEF message can read f...
Hi FabriceIndeed RF_enable has to be set to 1 in order to allow M24SR to answer to phone's requests. Otherwise the M24SR will stay mute with respect to RF NFC commands.The bit in the system file is only writable from the I2C side so the MCU, and is n...
Hello,I would encourage you to search for linux based SW development for communicating to M24SR through I2C.One example that can be found is a Raspberry Pi based interface to the M24SR Dynamic NFC tag, that can be found at: https://github.com/whaleyg...
Dear M24SR customerThe M24SR02 implements a communication mechanism through one Session token which is available either on the RF side or the I2C side, meaning that until the session token is released, only 1 side can have access to M24SR02. More det...