2021-06-21 06:45 AM
I cant seem to find the correct IDE, etc. Looking to use something like eclipse and the USB. Any good documentation would be helpful, thanks!
Solved! Go to Solution.
2021-06-21 08:38 AM
Hi RMurr.2,
it depends what you are pursuing. If you want to control the ST25R3911B-DISCO board from PC then there are two possibilities:
However if you want to develop something embedded I recommend to rather use X-NUCLEO-NFC05A1 + NUCLEO-L476 with one of
Best Regards, Ulysses
2021-06-21 08:38 AM
Hi RMurr.2,
it depends what you are pursuing. If you want to control the ST25R3911B-DISCO board from PC then there are two possibilities:
However if you want to develop something embedded I recommend to rather use X-NUCLEO-NFC05A1 + NUCLEO-L476 with one of
Best Regards, Ulysses
2022-03-02 07:32 AM
@Ulysses HERNIOSUS : can you please specify where exactly mentioned C# solution is located? After installing GUI I have folder c:\Program Files (x86)\STMicroelectronics\ST25R3911B_Discovery_GUI\ , but no any sources on C# included.
2022-03-02 07:52 AM
Hi,
C:\Program Files (x86)\STMicroelectronics\ST25R3911B_Discovery_GUI\Dll3911_Demos.sln.lnk
which should point to something like:
C:\Users\$(USER)\Documents\STMicroelectronics\ST25R3911B_Discovery_GUI\DLL_Demos\Dll3911_Demos.sln
BR, Ulysses
2022-03-02 09:05 AM
Ulysses, thank you, found!! But... why it's spreaded across the disk?? Isn't it logical to put everything under one folder? I lost my mind trying to find *.cs files. :[
2022-03-02 11:12 PM
Hi,
C:\Program Files... is generally not writable thus an MS Project cannot be compiled when installed there and user cannot make any source code changes. Thus the sources and project in a user folder - with a link on the installation to make finding it easier. It also has an entry in the StartMenu...
Maybe it could be made more obvious - how would you have found it?
BR, Ulysses
2022-03-07 04:45 PM
From my side it could be better to have everything under one folder. Believe you or not, but developers are not helpless kittens 🙂 they are able to copy project into own folder (they will move project anyway, so why to worry?) One unnoticeable Dll3911_Demos.sln.lnk is harder to see than search *.cs/*.sln files. Just my IMHO.