2017-11-03 07:30 AM
Hello, I'm using the RF Transceiver Demonstration Board, I connected it via USB, I successed in writing labview code that read/write messages via NFC to a device.
My question is: is it possible to connect more than one Demo Board and use them asynchronously ? I need to read/write NFC messages at least to two devices at the same time.
Thank you
Regards.
Massimo Ponte
#m24lr-discoverySolved! Go to Solution.
2017-12-15 08:02 AM
Hi Massimo,
If your question is about CR95HF-DEMO kit (embedded in the M24LR-DISCOVERY kit), it is not possible to use 2 readers via USB ports.
Best regards
2017-12-15 08:02 AM
Hi Massimo,
If your question is about CR95HF-DEMO kit (embedded in the M24LR-DISCOVERY kit), it is not possible to use 2 readers via USB ports.
Best regards