cancel
Showing results for 
Search instead for 
Did you mean: 

iOS 13 extendedReadMultipleBlocks still not working

DMugg.1
Associate II

Hi,

Is the command extendedReadMultipleBlocks on iOS 13 still not working?

When yes, do you know any news from Apple when this will be fixed?

I need this command now...

Thanks four your answers.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
victor laraison
ST Employee

yes, it is same. Issue is resolved in iOS14 beta2 as well !! :)

br,

View solution in original post

8 REPLIES 8
victor laraison
ST Employee

Hi,

I have to check with latest iOS13 beta release iOS 13.6 beta 2.

Apple updated us (2months ago) the bug status with "Resolution:Potential fix identified - For a future OS update".

I 'm coming back to you very soon...

victor laraison
ST Employee

Hi again DMugg,

So, I have re-tested with iOS13.6 beta2, and issue is always the same. So, it is still not working !!!!

Xfingers next week with iOS14 beta release...

Br,

wow that's just sad...Apple takes so much time to fix this issue!

Please update me with the iOS14 Beta next week.

Thanks in advance.

victor laraison
ST Employee

Hi Dmugg,

iOS14 beta2 version is fixing it !!

Hope it helps.

Br,

J.Brun
Associate II

Hello,

Do you know if it's the same problem to reading data when address requires 2 bytes (by example reading on a m24lr64-r tag). (Linked with this issue : https://community.st.com/s/question/0D50X0000B09Q8SSQU/example-of-using-the-new-ios-13-corenfc )

Morever, it is possible to see the bug report ? Or isn't public ?

Best regards,

victor laraison
ST Employee

yes, it is same. Issue is resolved in iOS14 beta2 as well !! :)

br,

victor laraison
ST Employee

bug report is not public.

J.Brun
Associate II

What a quick response ! :D

Thank you for that good news !

Best regards,