2020-06-18 04:08 AM
Hi,
Is the command extendedReadMultipleBlocks on iOS 13 still not working?
When yes, do you know any news from Apple when this will be fixed?
I need this command now...
Thanks four your answers.
Solved! Go to Solution.
2020-07-24 02:19 AM
2020-06-18 05:43 AM
Hi,
I have to check with latest iOS13 beta release iOS 13.6 beta 2.
Apple updated us (2months ago) the bug status with "Resolution:Potential fix identified - For a future OS update".
I 'm coming back to you very soon...
2020-06-19 12:29 AM
Hi again DMugg,
So, I have re-tested with iOS13.6 beta2, and issue is always the same. So, it is still not working !!!!
Xfingers next week with iOS14 beta release...
Br,
2020-06-19 12:32 AM
wow that's just sad...Apple takes so much time to fix this issue!
Please update me with the iOS14 Beta next week.
Thanks in advance.
2020-07-24 01:11 AM
Hi Dmugg,
iOS14 beta2 version is fixing it !!
Hope it helps.
Br,
2020-07-24 02:13 AM
Hello,
Do you know if it's the same problem to reading data when address requires 2 bytes (by example reading on a m24lr64-r tag). (Linked with this issue : https://community.st.com/s/question/0D50X0000B09Q8SSQU/example-of-using-the-new-ios-13-corenfc )
Morever, it is possible to see the bug report ? Or isn't public ?
Best regards,
2020-07-24 02:19 AM
yes, it is same. Issue is resolved in iOS14 beta2 as well !! :-)
br,
2020-07-24 02:19 AM
bug report is not public.
2020-07-24 02:23 AM
What a quick response ! :D
Thank you for that good news !
Best regards,