2020-04-20 11:00 PM
Hi,
We bought ST25RU3993-EVAL from your company. This evaulation board worked. I installed ST25RU3993 RS. I set Reader Settings,choosed Antenna. I did everything you told in video. You mentioned in your demo video that you can read up to 11 meters.
But i can read up to 50 centimeters. You used A0025 in your video. Is this about or is there something i missed?
Solved! Go to Solution.
2020-04-21 12:50 AM
Hello,
the antenna being used in the video (Poynting Patch A0025) is indeed a long range antenna.
The 13 meters shown in the video cannot be reached with the antenna provided with the ST25RU3993-EVAL
which is a near field antenna and is designed for short ranges.
best regards,
Cedric
2020-04-21 12:50 AM
Hello,
the antenna being used in the video (Poynting Patch A0025) is indeed a long range antenna.
The 13 meters shown in the video cannot be reached with the antenna provided with the ST25RU3993-EVAL
which is a near field antenna and is designed for short ranges.
best regards,
Cedric
2020-04-21 5:10 AM
Hello Cedric,
Thanks for answer. I have one more question :)
The distance I want to read 3 meters. Which Antenna Model would you recommend?
2020-04-23 10:04 AM
Hi Uyalç.1,
reaching a specific read distance depend on a number of things including the reader output power, environment, tag model, tag orientation, material the tag is mounted on.
Typically a link budget calculation helps you to figure out which antenna gain is required to establish the link and hence which antenna model.
I am guessing, and apologies I am wrong, you would like to run a quick test.
Consider A5020 from Times-7.
If this antenna does not fit your requirements e.g. size, you might browse their portfolio and/or look at Laird or MTI as well finding an antenna with a similar gain.
Cheers,
B