2020-07-27 4:15 AM
Hello!
I have been working with the NFC05A1 NFC Reader in combination with a G070RB, but am momentarily stuck on how to use it in my own program.
I have followed all the steps given in an other post with a person having close to the same issue: https://community.st.com/s/global-search/25R3911B?t=1595829552630
But I keep getting errors left and right on includes and functions, which makes me come to a question whether all of this is needed for just a 'simple' program.
My main question here is whether there is an easy way to implement a program to read the UID from an NFC Tag. It's all my program has to do, the example given in the X-CUBE-NFC5 seems a little too much for what I want it to do.
Kind regards,
Joey
Solved! Go to Solution.
2020-08-24 1:52 AM
Hi,
The CS signal is not properly driven: it should be low during a whole frame (e.g. low when sending the 03 03 polling command, in your trace the CS goes high in between). Make sure to have
SPI interface is not properly selected: in your IOC project, the SSI_0/Interface pin is not set. It should be 1 (see table 4 in the ST25R95 DataSheet). Make sure to have PC7 being defined as SSI_0 and being high.
The SPI baud rate is exceeding the max ST25R95 SPI clock frequency. It should not exceed 2Mbits/s (current value is 8...). Make sure to update the presscaler to 8 (==> Mbits/s) or 16 (==> 1 Mbits/s).
Rgds
BT
2020-08-24 3:13 AM
Hi Brian,
This made it work, I was looking at the documentation in the CR95HF Datasheet which seems incomplete regarding to the ST25R95 Datasheet, unless the IRQ_IN pin is not needed at all.
Kind Regards,
Joey