2024-01-10 7:10 AM
I'm using FP-SNS-SMARTAG1, but I can't write strings correctly with code, and I can't write anything, what should I do?
while (1)
{
/* Wake Up due to RTC timer */
if(WakeUpTimerInterrupt) {
WakeUpTimerInterrupt =0;
WakeUpTimerCallBack();
}
/* There are a RF activity */
if(RFActivity) {
RFActivity = 0;
DetectRFActivity();
}
SmarTag_LED_GREEN_On();
/* Init SmarTag sensor */
//InitSmarTagSensor();
//MEMS_Sensors_ReadData();
char str[] = "Hello, NFC!"; // String variable instead of string literal
const uint16_t address = 0x00;
const uint16_t size = strlen(str) + 1; // Include null terminator
// Call the NFC07A1_NFCTAG_WriteData function
SMARTAG1_NFCTAG_WriteData(SMARTAG1_NFCTAG_INSTANCE, (uint8_t *)str, address, size);
if(!WakeUpTimerIsSet) {
/* task executed, now can set next wakeup timer */
if(HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0, RTC_WAKEUPCLOCK_CK_SPRE_16BITS)!= HAL_OK) {
Error_Handler();
}
WakeUpTimerIsSet= 1;
}
#ifndef SMARTAG_ENABLE_DEBUG
/* -> Stop mode */
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
#else /* SMARTAG_ENABLE_DEBUG */
/* Wait Next event */
__WFI();
#endif /* SMARTAG_ENABLE_DEBUG */
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}