‎2019-06-30 2:54 AM
What is explanation for this code (0x81) - can not find it in documentation.
Receiving it for FS2JAST4 chip.
Solved! Go to Solution.
‎2019-07-01 2:38 AM
​Hi,
see https://community.st.com/s/profile/0050X0000089G09QAE for similar issue with nRF52.
Would it be possible to connect a logic analyzer on the SPI link and check the various timings? I suspect something wrong around SPI. Can you also check that the nRF52810 RF part does not cause some noise on the SPI link (i.e. make sure that the RF part is OFF for testing the SPI connection))
Rgds
BT
‎2019-07-01 1:03 AM
​Hi,
In order to better support you, would you please provide information about your HW and SW setup and about the issue:
Many thanks
Rgds
BT
‎2019-07-01 1:35 AM
Thanks for response =)
I am using my own pcb with nRF52810 and CR95HF (both from China) - connected via SPI. CR95HF report ID: NFC FS2JAST4
SW: Segger SAS 4.16 with nRF SDK 15.3
used commands:
idncommand[3] = {0x00, 0x01, 0x00};
setprotocolcommand[5] = {0x00, 0x02, 0x02, 0x01, 0x0F};
inventorycommand[5] = {0x00, 0x04, 0x02, 0x03, 0x2B};
readmultiblockcommand[7] = {0x00, 0x04, 0x04, 0x03, 0x23, 0x00, 0x02};
readblockcommand[6] = {0x00, 0x04, 0x03, 0x03, 0x20, 0x00};
with different hardware (own pcb Arduino/nRF51 + CR95HF from Mouser) - all works ok.
tested frequencies from 150k to 2M and modes 0 and 3 - no change in results.
0x81 response is from various commands - echo, inventory, read block, read multiple block.
Found:
when received 0x81 -> re-init SPI, wakeup CR95HF via IRQ, setup SPI, protocol select then repeat command -> no 0x81 - command executed and 0x80 received.
such behaviour is very frequent - aprox 99% of commands require such re-init procedure to perform correctly. After init/re-init - no more than 2 consecutive commands with 0x00/0x80 response, then 0x81
I suppose that it can be a "fake CR95HF" case with China IC....
‎2019-07-01 2:38 AM
​Hi,
see https://community.st.com/s/profile/0050X0000089G09QAE for similar issue with nRF52.
Would it be possible to connect a logic analyzer on the SPI link and check the various timings? I suspect something wrong around SPI. Can you also check that the nRF52810 RF part does not cause some noise on the SPI link (i.e. make sure that the RF part is OFF for testing the SPI connection))
Rgds
BT
‎2019-07-02 1:19 AM
Hi,
I guess you are managing the SPI Slave Select by software. Can you check that the setup time of the Slave Select is inline with the CR95HF datasheet §6.4. You may need to add some delay here.
Rgds
BT
‎2019-07-04 9:25 AM
Hi,
error 0x81 means Invalid command code. My feeling is that some data are corrupted on the SPI link.
Rgds
BT