cancel
Showing results for 
Search instead for 
Did you mean: 

Connection between STEVAL-SMARTAG1 and ST Link V2. Not able to detect the target board.

TChau.1
Associate II

I am using STEVAL-SMARTAG1 and ST Link V2 (https://www.st.com/en/development-tools/st-link-v2.html)

Find the connections in the image attached.

Please share details related to required connections, debugger configuration etc.

0693W00000D2k66QAB.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
TChau.1
Associate II

Hi,

Initially we connected it using the flat ribbon cable. Now we connected directly with jumper cables and it got connected.

Thanks for pointing out.

We can mark this thread as close.

View solution in original post

5 REPLIES 5
Brian TIDAL
ST Employee

Hi TChau.1,

have you properly followed the various steps described in §7 of UM2427, in particular step #1 "Insert a CR2032 battery in the battery holder on the back of the STEVAL-SMARTAG1 evaluation board to power the target microcontroller."?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TChau.1
Associate II

Hello,

We are following the UM2427 document, but the document shows the connections for debugger based on Nucelo development board and we are using the ST-Link/V2 (Find the image_1). Does this debugger supports this Board/microcontroller.

  • Yes, Step #1 is followed. CR2032 is connected.
  • With STM32 Cube Programmer, we are testing the setup and getting the following logs/error. (Refer image_2)
  • We tried with multiple combinations of Port(SWD/JTAG), Frequency, Mode and Reset Mode. Please suggest expected configuration.

Image_1 : 

0693W00000Dpe1XQAR.pngImage_2 :

0693W00000Dpe1cQAB.png

Brian TIDAL
ST Employee

Hi,

I see no reason to have STLink/V2 not supporting this MCU. It should work in SWD configuration.

Have you connected the STEVAL-SMARTAG1 to the STLink/V2 flat ribbon or directly on the STLink/V2 PCB 20 pins connector? Can you check that the connection is not "mirrored" ?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TChau.1
Associate II

Hi,

Initially we connected it using the flat ribbon cable. Now we connected directly with jumper cables and it got connected.

Thanks for pointing out.

We can mark this thread as close.

Brian TIDAL
ST Employee

Well done! Thanks for your feedback.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.