cancel
Showing results for 
Search instead for 
Did you mean: 

Comparing low power card detection between ST25R210/300/500 and ST25R39xx

OliM
Senior II

Since the 210 reader seems to be cheaper and smaller (in non BGA package) than the 3916b we are currently using, while delivering comparable output power, I am naturally intrigued.  
But the wakeup mode figures don't quite impress, even though it is advertised for situations "where each µA matters".

Wake-up mode for the ST25R300, ST25R500, ST25R501 and ST25R210 - Application note

gives a 75.17 μA figure for 200ms scanning (using 250mA Amplitude)
Wake-up mode for ST25R3916/16B, ST25R3917/17B, ST25R3918, ST25R3919B, and ST25R3920/20B devices - Application note
gives  a 43.74 µA figure for 200ms scanning (using 200mA Amplitude)

Even adjusted for the amplitude difference, that would give >35% more power draw for the 210. Is there a way this is compensated through higher sensitivity, so actually we need less Amplitude on the 210, or should I really expect a regression in low power card detection?

1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee

Hi,

these two example numbers cannot be really be compared:

  • 200mA vs 250mA: depends on application matching / chosen regulator setting (as already discovered by you)
  • Tmeas: 25us vs 43.7us: On R210/300/500 it can be easily be adapted between 10.7 and 43.7 (with tagdet_len even up to 61.4us)

Without having done the math in detail I expect with similar Tmeas and similar amplitude also similar power consumption. Compared to ST25R39xx I expect much more sensitivity.

You can even further reduce Tmeas and see if it affects noise floor and thus also sensitivity.

BR, Ulysses

 

View solution in original post

1 REPLY 1
Ulysses HERNIOSUS
ST Employee

Hi,

these two example numbers cannot be really be compared:

  • 200mA vs 250mA: depends on application matching / chosen regulator setting (as already discovered by you)
  • Tmeas: 25us vs 43.7us: On R210/300/500 it can be easily be adapted between 10.7 and 43.7 (with tagdet_len even up to 61.4us)

Without having done the math in detail I expect with similar Tmeas and similar amplitude also similar power consumption. Compared to ST25R39xx I expect much more sensitivity.

You can even further reduce Tmeas and see if it affects noise floor and thus also sensitivity.

BR, Ulysses