2020-07-07 6:18 AM
Hello,
My design must be very low power consuming. So, I am intended to reach 50 uA while waiting for a card by using the Tag detection mode.
Is there any other approach so as to decrease those 50 uA while waiting for a transponder?
Reagards, Ramon
Solved! Go to Solution.
2020-07-07 8:38 AM
Hi,
the tag detection mode is supported in the ST25R95/CR95HF RFAL. It is demonstrated in the X-CUBE-NFC3 polling demo.
See AN3433 (Optimization of wake-up time and power consumption on ST25R95 and CR95HF devices) for detail information about low power mode.
For your information, the IRQ_OUT interrupt is raised by the ST25R95/CR95HF when exiting the low power mode (i.e. when a tag is in the operating field). This can be used to wake up the host MCU from its low power mode.
Rgds
BT
2020-07-07 8:38 AM
Hi,
the tag detection mode is supported in the ST25R95/CR95HF RFAL. It is demonstrated in the X-CUBE-NFC3 polling demo.
See AN3433 (Optimization of wake-up time and power consumption on ST25R95 and CR95HF devices) for detail information about low power mode.
For your information, the IRQ_OUT interrupt is raised by the ST25R95/CR95HF when exiting the low power mode (i.e. when a tag is in the operating field). This can be used to wake up the host MCU from its low power mode.
Rgds
BT