2021-06-30 1:57 AM
Hello all
I use ST25DV64K.
I am always set the MB_MODE of ST25DV64K to 1 after power-on
After setting the value to 1, a verify check is performed to confirm that the value is set to 1.
And the result MB_MODE is 1.
When the power is turned on again after the above operation, MB_MODE is always set to 0.
Since MB_MODE is the "System configuration area", I thought MB_MODE is 1, but MB_MODE is 0.
Is this the correct behavior of the ST25DV?
Also, is there an explanation of this behavior in the datasheet (st25dv64.pdf)?
BR
Morooka
Solved! Go to Solution.
2021-07-08 7:47 AM
Hello Morooka,
The MB_CTRL_Dyn register is a volatile regsiter, and will always be set to 0 at boot time.
The MB_MODE is a static configuration register that is non-volatile, and value is kept upon reboot.
Now, the MB_MODE is not linked to the value of MB_EN bit in MB_CTRL_Dyn register.
Here is how it works:
If MB_MODE=0, it is forbidden to write in MB_CTRL_Dyn register.
If MB_MODE=1, it is allowed to write in MB_CTRL_Dyn register.
MB_CTRL_Dyn is used to enable the mailbox (so called Fast Transfer Mode), on demand during a session, by writing the MB_EN bit to 1.
By default, the device always boots with mailbox disabled, meaning MB_EN=0 in MB_CTRL_Dyn register.
So, if you want to use the mailbox after boot, you have to explicitly write MB_EN=1 in MB_CTRL_Dyn.
Hope this is more clear now.
Best regards.
2021-07-04 8:05 PM
I'm sorry.
The register is not MB_MODE, but MB_EN(bit0) of MB_CTRL_Dyn register.
So, will the MB_EN bit of the MB_CTRL_Dyn register be set to "0" when the power is turned on?
Even if the MB_MODE register is '1', will the MB_EN bit in the MB_CTRL_Dyn register remain '0'?
BR
Morooka
2021-07-08 7:47 AM
Hello Morooka,
The MB_CTRL_Dyn register is a volatile regsiter, and will always be set to 0 at boot time.
The MB_MODE is a static configuration register that is non-volatile, and value is kept upon reboot.
Now, the MB_MODE is not linked to the value of MB_EN bit in MB_CTRL_Dyn register.
Here is how it works:
If MB_MODE=0, it is forbidden to write in MB_CTRL_Dyn register.
If MB_MODE=1, it is allowed to write in MB_CTRL_Dyn register.
MB_CTRL_Dyn is used to enable the mailbox (so called Fast Transfer Mode), on demand during a session, by writing the MB_EN bit to 1.
By default, the device always boots with mailbox disabled, meaning MB_EN=0 in MB_CTRL_Dyn register.
So, if you want to use the mailbox after boot, you have to explicitly write MB_EN=1 in MB_CTRL_Dyn.
Hope this is more clear now.
Best regards.
2021-07-09 12:49 AM
Hello JL.Lebon,
Thank you for your reply.
I understand about MB_MODE and MB_CTRL_Dyn register.
Thank you!!
Morooka