2018-02-23 09:44 AM
Hi there,
I would like to create a custom PCB build around the STSPIN32F0 MCU which integrates a gate driver and some other fancy features.
Now I need to know some specs of that driver but they're not listed in the Datasheet (or am I blind ? Maybe ...).
I need to know the resistance of the driver output for calculating if my MOSFETS will work with the driver ...
So what are the values for R_src and R_snk ?
Next thing I would like to know: I can't find a Power rating of the driver. Only thing that's mentioned in the datasheet is the 600mW of output current (sink / source).
Can anyone help me or point me into the right direction ?
Other solutions for calculating, wether my mosfets work are also welcome.Thank you in advance.#gate-driver #stspin32f0 #mosfet