2020-09-01 9:30 AM
2020-09-09 6:37 AM
@Rostyslav S ok, than I can suggest the BLDC 65 Motor
2020-09-08 1:19 AM
Hello @Rostyslav S
The EVSPIN32F0251S1 is able to drive three-phase permanent magnet synchronous motors (PMSMs) and brushless DC (BLDC) motors with compatible voltage and current ratings (see details below).
The board is a 3-phase complete inverter based on the STSPIN32F0251 controller, which embeds a 3‑phase 250 V gate driver and a Cortex®‑M0 STM32 MCU.
The power stage features STD17NF25 MOSFETs, but can be populated with any IGBT or Power MOSFET in DPAK or powerFLAT 6x5 package.
The board has a single-shunt sensing topology, and both the field-oriented control (FOC) and sensored or sensorless 6‑step control can be implemented.
With the mounted components the maximum ratings of the board are the following:
2020-09-08 2:25 AM
Thank you, Cristiana. This information is already provided in board manual.
Actually I was looking for motor part numbers that were tested with this board.
The motor I am currently using matches above requirements (except rated power, so I have upgraded EVSPIN32F0251S1 to support 500W motors), but I am not able to start it spinning. So I am looking for a motor that was specifically tested with this board and it 100% works.
2020-09-09 5:37 AM
Hi @Rostyslav S (Community Member) are you targeting a sensored or sensorless application?
2020-09-09 5:40 AM
@Cristiana SCARAMEL Eventually I am planning to use this board with for sensored application. But for now I want to start with running any motor with this board.
2020-09-09 6:37 AM
@Rostyslav S ok, than I can suggest the BLDC 65 Motor