2022-08-10 1:51 AM
2022-08-11 10:47 AM
Welcome, @VUV.1, to the community!
No, unfortunately there is exactly one buck regulator in this package in the STMicroelectronics portfolio - the ST1S12G12R.
We are very sorry, but with the still extremely high worldwide demand, no one can provide alternatives or other capacities in the medium or short term. The only option at the moment is to order very proactively and for the long term.
Does it answer your question?
Regards
/Peter
2022-08-11 10:52 PM
2022-08-12 12:31 AM
I completely understand your problem, but it is often ignored that the manufacturing process of a semiconductor component is an extremely complex one.
When the Corona pandemic started, many people stocked up on toilet paper and it was only available on allocation for a long time, if at all. In the case of toilet paper, the problem was solved quite quickly, but a new factory for semiconductor components takes several years until new components tumble out of the back. Unfortunately, this time is not over yet, which is why the current problem is not only at STMicroelectronics, but worldwide. By the way, the manufacturers of machines for chip production have the same problem, so we are chasing our own tail.
I am very sorry not to be able to give more positive news.
If the problem is resolved or answered, please mark this thread as answered by selecting Select as best. This will help other users find that answer faster.
Good luck!
Regards
/Peter