cancel
Showing results for 
Search instead for 
Did you mean: 

VNS3NV04DPTR-E this part is recommended by ST against VNS3NV04D-E, Where I can buy it, what is lead time.

VMali.1
Associate

I am looking for alternate for VNS3NV04D-E, please confirm VNS3NV04DPTR-E is suitable alternate? what is buying source & manufacturer lead time.

8 REPLIES 8
Peter BENSCH
ST Employee

Welcome, @VMali.1​, to the community!

Yes, the VNS3NV04DPTR-E can directly replace the obsolete VNS3NV04D-E, the parameters are identical. However, it is your responsibility to re-check any necessary approvals.

No one in this technical forum can give you a source of supply, so please contact your local distributor

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Hello Peter, Can you suggest any other alternative for VNS3NV04D-E<>, which can be easily avaialble. (package & pin differences are allowed) Thanks & Regards, VIvek Mali

Not really - the only dual low side switch being a bit similar is the VNLD5090-E, but its current limit is much higher. You can buy it directly from estore.st.com.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
vmali.11
Associate II

VNS3NV04D-E is tube packaging with NRND & VNS3NV04DPTR-E  is tape & reel with Active status, can we consider VNS3NV04DPTR-E  with 6-8 year life span..

vmali.11
Associate II

also same for  VNLD5090-E is not active for purchase link VNLD5090TR-E is available. Please confirm. End of life for VNLD5090TR-E also

VNS3NV04DP-E is not in the Product Longevity program, so long-term availability cannot be guaranteed or stated.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

VNS3NV04D-E is tube packaging with NRND & VNS3NV04DPTR-E is tape & reel with Active status, can we consider VNS3NV04DPTR-E with 6-8 year life span?.

also same for VNLD5090-E is not active for purchase link VNLD5090TR-E is available. Please confirm. End of life for VNLD5090TR-E also?

VNLD5090TR-E as active and in full production. It is also not part of the Product Longevity program, so long-term availability cannot be guaranteed or stated either.

As already mentioned, this is a technical forum. For statements on stock availability, please always contact the respective supplier/distributor, as stock can change daily.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.