cancel
Showing results for 
Search instead for 
Did you mean: 

�?VNH5019ATR-E】Motor Control IC Technical Question Can you please answer the questions in red and red boxes in the attached schematic?

KIshi.3
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @KIshi.3​ , to the comminity!

I'll just repeat the questions to make them easier to read:

Is it possible that -1.5V is applied to the CPU for all IN, OWM, DIAGx/ENx?

  • Yes, in case of negative transients it is possible that -1.5V will be present on all control pins.

Does this countermeasure rely on the parasitic diode protection of the CPU?

  • There are parasitic p-n junctions (diodes) at the MCU pins, but they are usually not intended to be used for protection. The protection resistor Rprot on the one hand limits the current for such a negative transient at Vbat and on the other hand protects the controlling MCU from latching-up.

Are there any pull-down resistors in each input port?

  • If you mean the input pins of the VNH5019ATR-E: no, there are no pull resistors.

Regars

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @KIshi.3​ , to the comminity!

I'll just repeat the questions to make them easier to read:

Is it possible that -1.5V is applied to the CPU for all IN, OWM, DIAGx/ENx?

  • Yes, in case of negative transients it is possible that -1.5V will be present on all control pins.

Does this countermeasure rely on the parasitic diode protection of the CPU?

  • There are parasitic p-n junctions (diodes) at the MCU pins, but they are usually not intended to be used for protection. The protection resistor Rprot on the one hand limits the current for such a negative transient at Vbat and on the other hand protects the controlling MCU from latching-up.

Are there any pull-down resistors in each input port?

  • If you mean the input pins of the VNH5019ATR-E: no, there are no pull resistors.

Regars

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.