2026-06-02 7:12 PM
Hello.
I am creating a motor control project for the EVSPIN32G4 using MotorControl Workbench 6.4.1.
The EVSPIN32G4 board definition provides configurations for "ThreeShunt_RawCurrents_SingleEnded_ExternalGain" and "ThreeShunt_RawCurrents_SingleEnded_InternalGain," but the current sensing section in the circuit diagram of this board appears to match the "ThreeShunt_RawCurrents_Differential_ExternalGain" configuration.
However, adding this configuration causes MotorControl Workbench to fail with an error. This is likely because the definition for "ThreeShunt_RawCurrents_Differential_ExternalGain" does not exist for the STSPIN32G4 in "MC_SDK_6.4.1\Utilities\PC_Software\STMCWB\assets\ConnectionParameters.json".
1. Why is it that the EVSPIN32G4 schematic shows a differential configuration, but the board definition only provides a single-ended option?
2. Is it possible to edit "ConnectionParameters.json" and add the "ThreeShunt_RawCurrents_Differential_ExternalGain" definition to use this configuration in MotorControl Workbench?
Thanks in advance and best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.