2023-01-29 6:19 AM
Hi Team, we are using VIPER16LN in one of our project. we are facing thermal shut down happening within 2mnts time. the below are the testing condition
Input voltage: 230VAC
Output Voltage : 15V
Output current: 250mA
But viper16LN can handle around 6W power as per the datasheet. and as per the edesign suit also at the above power the temperature rise of VIPER is 30 degrees only.
verified the circuit as edesign suit as well. but there is no improvement.
Please share your feedback.