cancel
Showing results for 
Search instead for 
Did you mean: 

Manual rotation of the stepper motor shaft to start the PowerSTEP01 controller.

Odyss
Associate

I wonder if it is possible without external sensors by manually rotating the stepper motor shaft to initiate the PowerSTEP01 controller. Manual rotation of the shaft triggers the controller while informing it of the motor's direction of operation. After this trigger, the specified sequence of work is executed after which the system goes into standby and waits for the next manual trigger of work.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0