2023-06-22 07:10 AM
At 350V dc voltage, Viper16 output is toggle for 2 s to 0V. What could be problem? ..... Output req 24V @ 250mA and Input 200V to 350V DC.
2023-06-25 08:35 AM
There could be several reasons for this. You have not posted any measurement results (oscillograms with galvanically separated oscilloscope), but first of all it looks as if the VIPER16 goes into thermal shutdown and restarts after cooling down. Because at 350V DC you are already quite far at the upper limit of the maximum output power, this could be due to the layout, the buck coil, the free-wheeling diode, etc.
Regards
/Peter