cancel
Showing results for 
Search instead for 
Did you mean: 

Viper115 cannot produce the required current

Mnemonic
Associate III

I am designing a new SMPS for my project I need 350mA at 15V but I could not get more than 100ma. when I reach to 100mA output voltage was start to decrease. when current goes to 200mA, output is like a sinusodial signal from 9v to 15V. I design my SMPS with E-design suit but its not working stable. I need urgent help

 

Mnemonic_0-1717402436350.png

 

11 REPLIES 11

Hi @Peter BENSCH 

I was changed my topology to Viper222XS because of your heat suggestion. But I have same problem with new IC

I was built my project with belowed shema but when its going to shutdown when current is going to 400mA. My circuit is start with 100mA but when pust to start button its going to 400mA immidiatly ( its like inrush current) and Viper will going to shutdown and start again 1Sn later

 

is there anywhy to disable over current protection ? 

Just I could not find 1.2mH coil and I was used 1mH coil with belowed datasheet

 

https://cdn.ozdisan.com/ETicaret_Dosya/514828_7988607.pdf

 

Mnemonic_0-1718010206237.png

Mnemonic_2-1718010573965.png

 

 

Mnemonic_1-1718010530865.png

 

 

Mnemonic
Associate III

Can anyone help about this problem

@AScha.3 @Peter BENSCH