2025-04-11 4:54 AM
Hi,
I'm trying to spec a fully integrated H-bridge for driving a small motor taking up to 6A nominal, with spikes up to 12A (looking at the VNHD7012AY, VNHD7070AY, and the VNH7100BAS). There are a lot of numbers for current limitation on the ST datasheets that I've come across and I haven't been able to find an explanation for. How should I interpret all of these, and how are each of these numbers obtained?
Specifically, I'm looking at:
- Continuous maximum output current I_max
- High-side current limitation I_lim_h
- Shutdown low-side current I_sd_ls
- Output saturation current I_out_sat (under Current Sense)
Solved! Go to Solution.
2025-04-11 6:10 AM
Welcome @joshlian, to the community!
Let me try to explain these values:
Does it answer your question?
Regards
/Peter
2025-04-11 6:10 AM
Welcome @joshlian, to the community!
Let me try to explain these values:
Does it answer your question?
Regards
/Peter
2025-04-11 6:31 AM
It does thank you very much!
2026-02-26 12:48 AM
So how about 12A and 15A mean in the VNH7100BAS datasheet?
2026-02-26 1:56 AM
With a fully protected H-bridge driver, it is somewhat difficult to make a concrete statement regarding the current, which is why I have attempted to break it down a little above. Also consider the resulting power loss of up to P = (12A)²*120mohms = 17.28W, which in the case of the high-side driver (depending on the test environment with 32K/W or 40.7K/W) would result in a temperature difference of up to 703K during static operation. For this reason, this current of 12A can only flow when the driver is under very short-term load.