Skip to main content
Explorer
April 10, 2025
Question

STEVAL-A6986IV3 grounding capacitors

  • April 10, 2025
  • 1 reply
  • 303 views

Hello,

I am strongly considering using the STEVAL-A6986IV3 based design for a 4 channel isolated gate driver power supply.  One thing that looked strange in the the schematic was the four ground capacitors Cgnd1,2,3,4 which are 4.7nF 2000V rated. These connect the ground on each isolated channel to the ground on the input supply voltage. Can someone explain the purpose of these? It seems counter intuitive that we would want to capacitively couple the grounds together on a isolated supply. 

Regards,

Jason

 

This topic has been closed for replies.

1 reply

RobK1
Associate II
April 11, 2025