2016-09-28 02:34 PM - last edited on 2023-08-31 12:02 AM by Peter BENSCH
Posted on September 28, 2016 at 23:34
hi
i am working on lighting dimmer.i want to protect triac when load is short.
so how can i do ?????
thank you
#triac
2016-12-06 12:54 AM
Hello Medhi,
Triac is a device that is automatically turned off at the zero current when not drived by a gate current. No way to turn the device off when the current is flowing.
Even if the Triac technology allows high current robustness compare to MOSFET technology, if a short-circuit of the load appears when the Triac is ON, the way to protect the Triac is to add a fuse in series with the Triac and the load.
To design the fuse and to be sure that the Triac can withstand safely the high current before the cut-off event, take a fuse with a I²t parameter below the Triac specified I²t (see datasheet of your Triac).
Hope it helps,
Best RegardsBenoit2017-01-26 03:01 AM
HI
renard.benoit
this is ture that when the triac is on and short circuit is occur so triac will be destroy.
now i am working on mosfet. it is working very good
thank you for replay.
2017-01-26 05:26 AM
Hello Medhi
You're welcome.
Additionnal thinks regarding your choice:
To protect MOSFET against load short-circuit you need a specific complex circuit, monitoring the current with a shunt (with losses) to turn off the MOSFET in its SOA.
That's why the Triac is often preferred for dimmer purpose.
Others MOSFET drawbacks compare to Triac are: high power losses, price for a same current rating device, or very poor withstanding to lightning surge (Huge MOV is required)...
My advice is to reconsider your choice.
Moreover, according to your application requirement, a fuse is often mandatory for safety purpose, then no additionnal device/circuit to protect the Triac.
Hope it helps
Benoit
2017-01-26 07:08 AM
HI
renard.benoit
yes. triac is better for dimmer. but i can not use fuse in my board. so when short circuit will be
occur the triac will be destroy.now i use this schamatic. but with different part number.
line voltage in 220 volt rms with 311 volt peak.
load current is 3 amper.
so which parameter (rms or peak) should be to consider when read the datasheet and study soa curve ?
thank you