cancel
Showing results for 
Search instead for 
Did you mean: 

Earth short protection TDA7498E

just280
Visitor

Hi, any suggestions to protect the speaker outputs of the TDA7498 from a short to mains supply earth?

Thanks!

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome @just280, to the community!

If the supply voltage of the TDA7498 is galvanically isolated from mains, there should be no problem if one of the speaker output wires is connected to mains supply earth.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Not sure that's a practical solution on a 170VA linear supply?  

Well, such a linear supply must also be galvanically isolated for safety reasons, or do you not have such isolation? Therefore the previous statement still applies.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.