cancel
Showing results for 
Search instead for 
Did you mean: 

TCPP03 compatibility with FETs that have a low Vgs(min)

rcoleman99
Associate II

We are looking at using the TCPP03 and TCPP01 for a system with a dual-role power port and a sink port. We want to use this dual MOSFET with both ICs (a dual MOSFET is needed for the TCPP01 to prevent backflow): https://fscdn.rohm.com/en/products/databook/datasheet/discrete/transistor/mosfet/aw2k21ar-e.pdf

 

The MOSFET has a Vgs(min) of -2V. There isn't much information about the gate driver circuits in the TCPP01/TCPP03 datasheets. Does the integrated gate driver drive below 0V when turning the gate off?


Thanks

1 REPLY 1
Didier HERROUIN
ST Employee

Dear Rcolemann99,

The GATE pin from the TCPP01/03 is driven between 0V and 5V.

No negative voltage is present on this pin.

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.