2024-08-02 07:30 AM
We have integrated the STWLC38 into our wireless power receiver design and are aiming to utilize the full 15W power capability. However, we have encountered an issue when using the latest QI2 (MPP) chargers. Our receiver remains in BPP (5W) mode, and we are unable to achieve EPP (15W) as desired.
Interestingly, when we use an older transmitter development kit (P9242-R, now obsolete), we are able to achieve EPP (15W) without any issues. We are keen to understand why this discrepancy exists with the newer QI2 chargers and how we can resolve it.
Additionally, we prefer to use QI2 chargers in our setup due to the presence of a metal ring that ensures proper alignment. Could you please provide guidance on how we can achieve EPP (15W) with QI2 chargers using the STWLC38?
Furthermore, do you have any plans to support the MPP protocol for the STWLC38 in the future? We have noticed that NXP now supports this protocol with their MWPR1516.
Thank you and best regards,
Olivier
Solved! Go to Solution.
2024-08-04 07:38 PM
Hi olivier
QI2 (MPP) chargers 15W is MPP protocol and STWLC38 only support EPP 15W. We have other WLC device which support MPP 15W.
2024-08-04 07:38 PM
Hi olivier
QI2 (MPP) chargers 15W is MPP protocol and STWLC38 only support EPP 15W. We have other WLC device which support MPP 15W.
2024-08-05 11:11 PM
Hi willzhou,
I'm experiencing a similar problem. I am trying to understand what you said. Are you saying that STWLC38 will not receive 15w EPP with Qi v2.0 transmitters?
Thanks,
Robert
2024-08-05 11:17 PM
Hi
If QI 2.0 TX support MPP and EPP, WLC38 can work with EPP 15W.
If QI 2.0 TX only support MPP, WLC38 only work at BPP 5W.
2024-08-07 07:15 PM
we can provide RX MPP module from our vender, you can combination this stamp board to your product.
2024-08-07 08:47 PM
I am interested in the RX MPP module. Could you provide me some more information?
2024-08-08 01:19 AM
add stamp example picture
2024-08-09 10:33 PM
What is the model number of the RX MPP module? Can you share the datasheet?
2024-08-20 02:27 AM
I will reach you in the email.