2024-08-06 11:25 PM
Hi ST community
The STWBC2-HP can be used with a GUI for configuration and plotting voltages and currents. The communication between GUI and firmware is done by UART. Is there any command list available that I can program my own interface on the computer? Unfortunately the ST support was not very helpful in this case.
Michael
2024-08-06 11:27 PM
Hi Michael
May i know which command you like to use?
STWBC2 UART command is for GUI use only.
2024-08-06 11:31 PM
Hi Will
I would like to use the commands to get the values which are available in the charts.
Michael
2024-08-06 11:39 PM
Hi
Sorry, This command is not open to customer.