2024-11-19 10:18 PM
We try to use STUSB4761 for a 100W USB-PD Source.
Test setup includes our PCB with STUSB4761 as power source, an e-marked 5A rated cable and Acroname "USBHub3c Pro Edition" as power sink.
According to the log (see Attachement) of the USB PD communication, STUSB4761 advertises in the 5th PDO 20V/5A but if I try to select this PDO the request is rejected.
Is there anything wrong with this configuration?
2024-12-02 09:13 AM
either our stusb4500 with different cables, either equipment used for certification, listed under USB-IF
Best regards
2024-12-04 10:38 PM