2021-05-09 10:32 PM
Hi,
in STUSB4500 if we are planning to use the chip for Power delivery and communication enabling circuit, then will it be necessary to do adjustments in the Vbus when and external 3v3 is applied to the Vsys pin.
In case of a Power delivery available port, then the Vbus will be able to power up the Vdd.
But in case of a non PD cable comes in contact for communication, for the ATTACH and AB_side detection, wont we require an external power on the Vsys pin..?
whether the ATTACH and AB_ Side pin wont be sufficient for communication circuit triggering.?
Have anyone tried this usecase for the STUSB4500.?
DO you have any suggestions on the same..?
Please share your views on this..
---
Best regards,
Akshay Vavukkal
2021-05-11 10:28 PM
STUSB4500 can be supplied in 3 different ways.
In your application, the ways being used is to be supplied through the VDD and VSYS pins for applications powered by VBUS with a system power supply delivering 3.3 V.
There seems to be no need for adjustments in VBUS.
Please refer to STEVAL-ISC005V1, where VSYS is connected to 3V3.
2021-05-12 12:07 AM
Hi Winfred,
If I use Vsys as an external supply and do not give power for Vdd at all,
Will the STUSB negotiations take place ..?
Will the AB_Side output be obtained as cable Is connected in the port..?
---
Thanks & Regards,
Akshay V
2021-05-13 8:38 PM
>If I use Vsys as an external supply and do not give power for Vdd at all,
According to datasheet it shall also work properly, although in most cases STUSB4500 should be powered by VDD pin only.
>Will the AB_Side output be obtained as cable Is connected in the port..?
No. But, ATTACH pin can be used instead.
This pin is asserted when a valid source-to-sink connection is established.
2021-05-14 12:09 AM
hi.
AB_side denotes the orientation of the cable connected in the port, right..?
>>Since the ATTACH pin is valid only when a source to sink connection is established, can that be chosen as an ideal input for the Communication part..?
>>and also the mux switch can be selected based on the routing lines for the Receptacle.
so, the AB_side would be able to determine the orientation of the cable connected and hence would determine the communication path Mux switch to select the proper channel as per the direction of the cable attached.
>>Just wanted to know if the cable is attached to STUSB with power given in the Vsys, will the AB_Side pin output will be obtained..?
if the source to sink connection can not be attained, then Vdd wont be powered up, since there would be no Vbus, hence by powering up Vsys,would it be able to identify the orientation of CC pin through AB_side pin
2021-05-16 5:18 PM
Sorry for misreading. I though you were asking to read the attaching status from AB_Side pin.
Answer to the question shall be yes instead.
> so, the AB_side would be able to determine the orientation of the cable connected and hence would determine the communication path Mux switch to select the proper channel as per the direction of the cable attached.
That would be correct.
> if the source to sink connection can not be attained, then Vdd wont be powered up, since there would be no Vbus, hence by powering up Vsys,would it be able to identify the orientation of CC pin through AB_side pin
If the connection is not attained, shouldn't it be better not to provide any status including AB_Side?